- No : 21364
- Release Date : 2018/08/22 16:27
-
Print
FR-PA07
Can I perform the forward rotation and reverse rotation by pressing the FWD/REV key on the enclosure surface operation panel FR-PA07?
- Category :
-
Answer
The forward rotation and reverse rotation are enabled by pressing the FWD/REV key on the operation panel.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700