- No : 21366
- Release Date : 2018/08/22 16:27
-
Print
FR-PA07
How can I disable the dial operation except the frequency setting when using the enclosure surface operation panel FR-PA07?
- Category :
-
Answer
Operations cannot be enabled separately.
You only can disable or enable all the operations.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700