• No : 21669
  • Release Date : 2018/08/22 16:28
  • Print

A7AY

1. Can I switch the output to current by using the A7AY while the input is 0 to 10 V?  
2. Is the output current for 10 V input the rated current of the inverter?
Category : 

Answer

1. Yes.  

2. The standard set by Pr.56.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700