- No : 21672
- Release Date : 2018/08/22 16:28
-
Print
Full scale frequency
A full-scale 1 mA DC analog meter is connected between the terminals FM and SD. Can I change the full-scale frequency?
- Category :
-
Answer
You can change the full-scale value by changing Pr.55 (Frequency monitor reference).
The initial setting is 60 Hz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700