• No : 21677
  • Release Date : 2018/08/22 16:28
  • Print

Terminal

I want to use the inverter terminal 4 to operate the inverter at 85 Hz when 20 mA is input from the current 4 to 20 mA input.
Should I change the setting of Pr.125 (Terminal 2 frequency setting gain frequency)?
Category : 

Answer

Change Pr.126 (Terminal 4 frequency setting gain frequency).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700