• No : 21709
  • Release Date : 2018/08/22 16:29
  • Print

FR-Configurator

When I used the FR Configurator (FR-SW3-SETUP-WJ) setup software to read a stored file, the setting values were already entered.
Is it necessary to perform batch write again to reflect the setting values on the inverter?
Category : 

Answer

If the values are already entered in the setting column, performing batch write reflects the setting on the inverter.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700