- No : 21709
- Release Date : 2018/08/22 16:29
-
Print
FR-Configurator
When I used the FR Configurator (FR-SW3-SETUP-WJ) setup software to read a stored file, the setting values were already entered.
Is it necessary to perform batch write again to reflect the setting values on the inverter?
- Category :
-
Answer
If the values are already entered in the setting column, performing batch write reflects the setting on the inverter.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700