- No : 21716
- Release Date : 2018/08/22 16:29
-
Print
Monitor indicator
How should I set the inverter to check the rotations per minute on its monitor?
- Category :
-
Answer
Set Pr.37 (Speed display) to the speed obtained when operating the machine at the frequency set with Pr.505 (Speed setting reference). (For FR-F700/E700/D700, set the speed obtained when operating the machine at 60 Hz.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700