- No : 21736
- Release Date : 2018/08/22 16:29
-
Print
Frequency setting
I use the inverter's terminal 4 to input the current 4 to 20 mA DC. However, the frequency setting value gets misaligned around the middle of the input range.
Can I adjust it?
- Category :
-
Answer
You cannot calibrate the frequency around the middle of the current input range.
The inverter determines the top and bottom points in the bias/gain adjustment, links these two points with a straight line, and calculates the frequency setting value against the input current.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700