- No : 21737
- Release Date : 2018/08/22 16:29
-
Print
Frequency setting
How can I set the running frequency to 120 Hz or higher?
Use the setting dial of the inverter to set the frequency.
- Category :
-
Answer
Change the value of Pr.18 (High speed maximum frequency).
You can set any frequency within the range defined by Pr.18.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700