- No : 21741
- Release Date : 2018/08/22 16:29
-
Print
Frequency setting
I want to change the running frequency but pressing the PU/EXT button on the operation panel does not change the operation mode to the PU mode.
Currently, a start command is externally sent and the frequency is set with the setting dial.
The PU, EXT, and MON LEDs on the operation panel are ON.
- Category :
-
Answer
From the LED, it is considered that the operation mode Pr.79 is set to "3".
The PU and EXT LEDs turn ON with this setting.
In this state, you cannot change between PU and EXT.
To set the frequency, turn the setting dial in the current operation mode to set the frequency and press the SET key to accept it.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700