- No : 21744
- Release Date : 2018/08/22 16:29
-
Print
Frequency setting
Which parameters should I use to set the maximum frequency?
- Category :
-
Answer
Pr.1 (Maximum frequency) and Pr.18 (Maximum frequency).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700