- No : 21744
- Release Date : 2018/08/22 16:29
- 
          
              Print
          
        
 
Frequency setting
    
      Which parameters should I use to set the maximum frequency?
    
  
    - Category : 
- 
      
    
 
    Answer
  
    Pr.1 (Maximum frequency) and Pr.18 (Maximum frequency).  
  
    
      
        - Product Name
- Inverter, magnet motor drive
        - Product Category
- Inverter
        - Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700