• No : 21768
  • Release Date : 2018/08/22 16:29
  • Print

Parameter setting

I want to install a full-scale 100 Hz frequency meter.
Which parameter should I set for this purpose?
Category : 

Answer

Set Pr.55 (Frequency monitor reference) to "100 Hz".
If the indication of the installed frequency meter does not match the running frequency, use the calibration parameter Pr.C0 (FM terminal calibration) to adjust it.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700