- No : 21772
- Release Date : 2018/08/22 16:29
-
Print
Multi-speed setting
What are the priorities between multi-speed settings?
- Category :
-
Answer
Priorities are: Low speed (RL) > Middle speed (RM) > High speed (RH).
For example, if the low speed (RL) and middle speed (RM) signals are input simultaneously, the low speed (RL) signal is prioritized.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700