- No : 21773
- Release Date : 2018/08/22 16:29
-
Print
Multi-speed setting and external potentiometer
What are the priorities between multi-speed setting and external potentiometer?
- Category :
-
Answer
The multi-speed setting is prioritized.
The external potentiometer setting is effective when the multi-speed signal is not input.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700