• No : 21775
  • Release Date : 2018/08/22 16:29
  • Print

Operation panel

I input the start signal via the terminal STF and set the frequency using the setting dial. I set Pr.161 (Frequency setting/key lock operation selection) to "1" (potentiometer mode) and Pr.79 (Operation mode) to "3".
When I press the "STOP" key on the operation panel, the motor is decelerated to stop and "PS" and "0.00" blink on the monitor. What happened?
Category : 

Answer

This is because the protective function works to stop the motor. It is not a fault indication.

To cancel the protective function, turn OFF the start signal and press the "PU/EXT" button.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700