- No : 21779
- Release Date : 2018/08/22 16:29
-
Print
Output current value
Can I change the detection level of the output current value using a potentiometer or something similar?
- Category :
-
Answer
The detection level of the output current value cannot be changed using a potentiometer or a similar device.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700