• No : 21817
  • Release Date : 2018/08/22 16:29
  • Print

External installation<br>Rated current

Answer

Since the external thermal prevents the motor from being overheated, install it between the output terminal of the inverter and the motor.
The rated current is the maximum current value that can continuously and safely flow through the inverter.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700