- No : 21818
- Release Date : 2018/08/22 16:29
-
Print
Operation mode setting value
When inputting the start command and frequency setting command for operation externally, which value should be set to Pr.79 (Operation mode)?
- Category :
-
Answer
Set Pr.79 to "2" (external operation mode).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700