- No : 21819
- Release Date : 2018/08/22 16:29
-
Print
Operation stop, frequency setting
The inverter does not operate.
I want to stop operation and set frequency with the inverter alone.
- Category :
-
Answer
Set Pr.79 (Operation mode) to "1" (PU operation mode).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700