• No : 21821
  • Release Date : 2018/08/22 16:29
  • Print

Running frequency

I operate the inverter by pressing the RUN key in the PU operation mode, but the running frequency does not increase over 120 Hz.  
Category : 

Answer

Check the setting of Pr.1 (Maximum frequency) and Pr.18 (High speed maximum frequency).
Pr.1 is initially set to "120 Hz".
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700