- No : 21842
- Release Date : 2018/08/22 16:29
-
Print
Frequency setting
I set the frequency to 40 Hz using the setting dial and operated the inverter.
After resetting the power, should I set the frequency again?
- Category :
-
Answer
When the frequency is set using the setting dial, it is not necessary to set it again.
The inverter memorizes the setting value internally even after the power reset.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700