- No : 21845
- Release Date : 2018/08/22 16:29
-
Print
Control terminal
Are the multiple terminals SD of the inverter all the same?
- Category :
-
Answer
Yes. (Terminal SDs are connected with each other inside of the inverter.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700