- No : 21864
- Release Date : 2018/08/22 16:29
-
Print
Terminal FM
Can I connect multiple meters (FS (full-scale 0 to 1 mA)) in series?
- Category :
-
Answer
No. This is because the current cannot flow if the total internal impedance of the meter connected to the terminal FM is 300 Ω or higher.
You can connect multiple meters if the total internal impedance of the meter is less than 300 Ω.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700