• No : 21886
  • Release Date : 2018/08/22 16:29
  • Print

CC-Link

How can I read inverter faults from the programmable controller in CC-Link operation?
Category : 

Answer

Create a ladder program to read inverter faults on the programmable controller.
Set the instruction code (H74-H77) and turn ON the instruction code execution request RYF.
Identify the fault record from the read code.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700