- No : 21913
- Release Date : 2018/08/22 16:30
-
Print
Frequency setting
Which parameter should be used to set the maximum value using the externally connected frequency setting potentiometer?
- Category :
-
Answer
Use Pr.125 (Terminal 2 frequency setting gain frequency).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700