• No : 22354
  • Release Date : 2018/08/31 14:33
  • Print

AX

Answer

AX (Auxiliary switch) is a switch which electrically displays the ON / OFF state.
The markings are 14/AXa, 12/AXb and 11/AXc.
* If the circuit breaker itself is ON state, 14/AXa and 11/AXc are conductive state.
* If the circuit breaker itself is OFF state or tripping state, 12/AXb and 11/AXc are conductive state.
Product Name
Internal Accessories
Series
WS-V