• No : 23290
  • Release Date : 2018/09/12 15:11
  • Print

About Low-voltage Power Distribution Products

What is the minimum applicale voltage and current at auxiliarycontact of SD-Q* type?
Category : 

Answer

The minimum applicable load voltage and current are as follows. Contactreliability is indicated by fault rate λ60 (Number of faults / Operatingcycles per one contact) at the reliability level 60%.1. Main contact: 24V300mA (Contact reliability 1*10-7/ time)2. Auxiliary contact: 5V3mA (Contact reliability 5*10-7/ time)
Product Name
Motor Starters
Series
MS-T/N