• No : 23320
  • Release Date : 2018/09/12 15:11
  • Print

About Low-voltage Power Distribution Products

What is the minimum applicable voltage and current of S-T*, SD-T*,SL-T*, SLD-T*, S-N*, SD-N*, SL-N* and SLD-N* type?
Category : 

Answer

The minimum applicable load is as follows. Contact reliability is indicatedby fault rate λ60 (Number of fault / Operating cycles per one contact) atthe reliability level 60%.1. Main contact: 48V200mA (Contact reliability 1*10-7/ time)2. Auxiliary contact: 20V3mA (Contact reliability 1*10-7/ time)
Product Name
Motor Starters
Series
MS-T/N