• No : 23351
  • Release Date : 2018/09/12 15:12
  • Print

About Low-voltage Power Distribution Products

What is the withstand voltage value of US-N* type?
Category : 

Answer

The withstand voltage of US-N5SS, US-N8SS, US-N70NS and US-N80NStype is 2kV. The withstand voltage of US-N20 to 50 type is 2.5kV. Theapplied points are as follows.1. Between a main circuit terminal and a control circuit terminal2. Between all live parts and ground3. Between each phase in a main circuit
Product Name
Motor Starters
Series
MS-T/N