- No : 23358
- Release Date : 2018/09/12 15:12
-
Print
About Low-voltage Power Distribution Products
What is the temperature of US-N* type cooling fins when carryingthe rated current?
- Category :
-
Answer
When carrying the rated current at ambient temperature of 40℃ (whencarrying the rated heater load), the maximum temparature of cooling finis approximately 100℃.
- Product Name
- Motor Starters
- Series
- MS-T/N