• No : 23441
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/26 16:57
  • Print

Ethernet connection with the QnUD(H)CPU

Answer

The following describes an example of settings to connect a GT27, GT25, or GT21 model (Ethernet connection model) and the QnUD(H)CPU by Ethernet by using QJ71E71-100.

1. Configure the following settings in GT Designer3 (GOT2000).
◆ For GT Designer3 (GOT2000) Version1.100E or later
 (1) Select [Common] → [Controller Setting] → [CH1] from the menu.
   Manufacturer: MITSUBISHI ELECTRIC
   Controller Type: MELSEC-Q/QS, Q17nD/M/NC/DR, CRnD-700
   I/F: Ethernet:Multi
   (For GT Designer3 (GOT2000) Version1.170C or earlier, Standard I/F(Ethernet): Multi)
   Driver: Ethernet(MITSUBISHI ELECTRIC), Gateway
   (For GT Designer3 (GOT2000) Version1.178L or earlier, Ethernet (MELSEC), Q17nNC, CRnD-700, Gateway)
   GOT Net No.: 1
   GOT Station: 18
 (2) Select [Common] → [Controller Setting] → [CH1] → [Ethernet Setting] from the menu.
   Host: *
   Net No.: 1
   Station: 1
   Unit Type: QJ71E71/LJ71E71
   IP address: 192.168.3.39
   Port No.: 5001
   Communication: UDP
 (3) Select [Common] → [GOT Ethernet Setting] → [GOT IP Address Setting] → [Standard Port] from the menu.
  (For GT Designer3 (GOT2000) Version1.170C or earlier, select [Common] → [Controller Setting] → [CH1] → [GOT Standard Ethernet Setting].)
   GOT IP address: 192.168.3.18
   Subnet Mask: 255.255.255.0

2. Configure the following settings in GX Works2.
 (1) Select [Parameter] → [Network Parameter] → [Ethernet/CC IE/MELSECNET] from the menu.
   Network Type: Ethernet
   Start I/O No.: 0000
   Network No.: 1
   Station: 1
 (2) Select [Parameter] → [Network Parameter] → [Ethernet/CC IE/MELSECNET] → [Action] from the menu.
   IP address: 192.168.3.39

For the details, refer to the following.

・ GOT2000 Series Connection Manual (Mitsubishi Electric Products) For GT Works3 Version1 (SH-081197ENG)
 "5.3 GOT Side Settings"
 "5.4 PLC Side Setting"
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (communication)
Series
GOT2000 Series