• No : 23477
  • Release Date : 2018/09/14 15:06
  • Update : 2025/10/09 18:20
  • Print

Displaying overlap windows in screen gesture mode

Answer

Overlap windows cannot be displayed in screen gesture mode. 
If a request to display the overlap window is received in the screen gesture mode, the overlap window is displayed after screen gesture mode is disabled.

* For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture), GOT function (standard function)
Series
GOT2000 Series, GOT3000 Series