• No : 23482
  • Release Date : 2018/09/14 15:06
  • Update : 2018/10/04 13:24
  • Print

Range of the screen display enlarged with the screen gesture function

How can I determine which part of the normal screen is currently displayed in the screen enlarged with the screen gesture function?
Category : 

Answer

◆ GT Designer3 (GOT2000) Version 1.105K or later
When the screen gesture mode is enabled, a frame indicating the screen gesture active area is displayed.
This frame consists of a bright red line only when the display contents inside the screen gesture active area are not enlarged, and a bright red line and dark red line when the display contents are enlarged. The length and position of the bright red line of the frame indicate where the enlarged display area corresponds the range in the full scale (100%) screen.

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture)
Series
GOT2000 Series