• No : 23482
  • Release Date : 2018/09/14 15:06
  • Update : 2025/10/09 18:35
  • Print

Range of the screen enlarged with the screen gesture function

How can I determine which part of the original screen is currently displayed on the screen enlarged with the screen gesture function?
Category : 

Answer

When screen gesture mode is enabled, a frame indicating the screen gesture active area is displayed. 
This frame is displayed with a bright red line only when the contents within the screen gesture active area are not enlarged, and with a combination of bright red and dark red lines when the contents are enlarged. The length and position of the bright red line of the frame indicates which area of the original screen (100%) is being enlarged. 

* For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture)
Series
GOT2000 Series, GOT3000 Series