FAQ
>
Human Machine Interfaces
>
Human-Machine Interfaces(HMIs)-GOT
>
GOT2000 Series
>
GT21
>
Using with the GOT1000 series on the network
Back
No : 23488
Release Date : 2018/09/14 15:06
Update : 2018/09/25 18:00
Print
Using with the GOT1000 series on the network
Can the GOT1000 series and GOT2000 series be used together on the network?
Category :
FAQ
>
Human Machine Interfaces
>
Human-Machine Interfaces(HMIs)-GOT
>
GOT2000 Series
FAQ
>
Human Machine Interfaces
>
Human-Machine Interfaces(HMIs)-GOT
>
GOT2000 Series
>
GT27
FAQ
>
Human Machine Interfaces
>
Human-Machine Interfaces(HMIs)-GOT
>
GOT2000 Series
>
GT25
FAQ
>
Human Machine Interfaces
>
Human-Machine Interfaces(HMIs)-GOT
>
GOT2000 Series
>
GT21
Answer
The GOT1000 series and GOT2000 series can be used together on the network if the network type is one of the following.
・ MELSECNET/H
・ CC-Link IE Controller Network
・ CC-Link IE Field Network
・ CC-Link (Intelligent device station/via G4)
・ Ethernet
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (communication)
Series
GOT2000 Series