• No : 23495
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/25 17:30
  • Print

Connecting the GOT2000 series and a barcode reader or other devices by USB

Can I connect a GOT2000 series model with a barcode reader, 2D code reader, or RFID by USB?
Category : 

Answer

You can connect a GOT2000 series model with a barcode reader or 2D code reader by USB.
RFID does not support USB connection.

Note that a barcode reader or 2D code reader to be connected to a GOT2000 series model is required to satisfy the following conditions.
 ・ A USB keyboard interface is provided.
 ・ A Japanese 106 keyboard or the English 101 keyboard is settable as the USB keyboard type.
 ・ "Enter" is settable as the terminator.

Also, GT Designer3 (GOT2000) Version 1.175H or later is required.
Version 1.170C and earlier do not support USB connection with a barcode reader, 2D code reader, or RFID.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Peripheral, GOT function (communication)
Series
GOT2000 Series