- No : 23558
- Release Date : 2018/09/14 15:09
- 
          
              Print
          
        
 
Battery error
    
      What devices in the Motion CPU are for battery errors?
    
  
    - Category : 
- 
      
    
 
    Answer
  
    The following shows the devices for the battery errors.
• [SM51] Battery low latch
  Turn ON when the voltage of battery reduces to less than 2.5[V].
  Remains ON even if the condition is restored to normal thereafter.
• [SM52] Battery low
  Turn ON when the voltage of battery reduces to less than 2.5[V].
  Turn OFF when the voltage of external battery returns to normal.
• [SM58] Battery low warning latch
  Turn ON when the voltage of battery reduces to less than 2.7[V].
  Remains ON even if the condition is restored to normal thereafter.
• [SM59] Battery low warning
  Turn ON when the voltage of battery reduces to less than 2.7[V].
  Turn OFF when the voltage of external battery returns to normal.
  
    
      
        - Product Name
- Motion controller
        - Series
- MELSEC-Q