- No : 23708
- Release Date : 2018/09/19 17:16
-
Print
A lighting condition of RUN
Let me know the light up condition of RUN.
- Category :
-
Answer
Because this relay derives the control power from input of the CT secondary current, when the input current falls below about 0.5 A for 2-phase input or about 0.7A for single-phase input, it will light out. When the current is around this range, because of fluctuation of current values, LED (RUN) will lights up/out repeatedly. That is not a failure.
- Product Name
- Protection Relay
- Series
- MELPRO-A Series