FAQ


FAQAbout Products
FAQ
UVT
What is UVT (Undervoltage Trip) ?
Answer
UVT is an internal accessory which trips a circuit breaker in the case that circuit voltage decreases from 70% to 35% or less, and turns it "ON" after resetting manually in the case that circuit voltage recovers to at least 85%. There are "Resettable type" which performs reset operation even with non-excitation and "Reset prevention type" which does not perform reset operation in non-excitation. The makings are D1/P1 and D2/P2.
Precaution for use is as below.
1. For UVT coil, you must apply specified voltage and then reset or make currents.
2. The number of trip durability is 10% of operating cycles of a circuit breaker.
3. You must not reset (Reset prevention type) or make currents (Resettable type) for a circuit breaker with UVT non-excitation because it result in a fault due to wear of tripping latch.
4. In UVT circuit, you must install Miniature circuit breaker or Fuse.
Precaution for use is as below.
1. For UVT coil, you must apply specified voltage and then reset or make currents.
2. The number of trip durability is 10% of operating cycles of a circuit breaker.
3. You must not reset (Reset prevention type) or make currents (Resettable type) for a circuit breaker with UVT non-excitation because it result in a fault due to wear of tripping latch.
4. In UVT circuit, you must install Miniature circuit breaker or Fuse.
- Product Name
- Internal Accessories
- Series
- WS-V