FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
FAQ
AL
What is AL (Alarm switch) ?
Answer
AL (Alarm switch) is a switch which electrically displays tripping state of a circuit breaker.
The markings of the switch are 8/ALa, 96/ALb and 95/ALc.
*When the circuit breaker itself is ON or OFF, 96/ALb and 95/ALc are conductive states.
*When the circuit breaker itself trips, 8/ALa and 95/ALc are conductive states.
The markings of the switch are 8/ALa, 96/ALb and 95/ALc.
*When the circuit breaker itself is ON or OFF, 96/ALb and 95/ALc are conductive states.
*When the circuit breaker itself trips, 8/ALa and 95/ALc are conductive states.
- Product Name
- Internal Accessories
- Series
- WS-V