Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • No : 22364
  • Release Date : 2018/08/31 14:33
  • Print

Rated current sensitivity

What is the actual operating leakage current compared with the rated residual operating current?
Category : 

Answer

Earth Leakage Circuit Breaker and Earth Leakage Relay operate at higher than 50% but not exceeding 100% of the rated residual operating current IΔn. The earth leakage current that Earth Leakage Circuit Breaker and Earth Leakage Relay operate is called "residual operating current".
Product Name
Earth Leakage Circuit Breakers
Series
WS-V

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries