FAQ


FAQAbout Products

- FAQ > Low-voltage Power Distribution Products > Low-voltage Circuit Breakers > Earth Leakage Circuit Breakers > Time Delay type at the maximum operating time
FAQ
Time Delay type at the maximum operating time
What is the operating time range of Time Delay type at the maximum operating time?
Answer
The maximum operating time of Time-delay type Earth Leakage Circuit Breaker can be switched to 0.45s, 1.0s and 2.0s. The operating time is:
* when it is 0.45s : between 0.15 and 0.45s
* when it is 1.0s : between 0.6 and 1.0s
* when it is 2.0s : between 1.2 and 2.0s
* when it is 0.45s : between 0.15 and 0.45s
* when it is 1.0s : between 0.6 and 1.0s
* when it is 2.0s : between 1.2 and 2.0s
- Product Name
- Earth Leakage Circuit Breakers
- Series
- WS-V