FAQ


FAQAbout Products
 
 - FAQ > Low-voltage Power Distribution Products > Low-voltage Circuit Breakers > Molded Case Circuit Breakers > AC Breakers used at DC circuit
FAQ
AC Breakers used at DC circuit
      Is it possible to use a circuit breaker for AC in DC circuit? And what will happen to circuit breaker if using that ?
    
  
Answer
    It is not possible to use a circuit breaker for AC in DC circuit. Since the Arc-Extinguishing 
Device structure of circuit breaker for DC is different from that for AC, it may not break short circuit current. Moreover, since tripping device specifications for some circuit breakers are different, it may not operate against overcurrent.
    Device structure of circuit breaker for DC is different from that for AC, it may not break short circuit current. Moreover, since tripping device specifications for some circuit breakers are different, it may not operate against overcurrent.
- Product Name
- Molded Case Circuit Breakers
- Series
- WS-V