Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • No : 22381
  • Release Date : 2018/08/31 14:33
  • Print

AC Breakers used at DC circuit

Is it possible to use a circuit breaker for AC in DC circuit? And what will happen to circuit breaker if using that ?
Category : 

Answer

It is not possible to use a circuit breaker for AC in DC circuit. Since the Arc-Extinguishing
Device structure of circuit breaker for DC is different from that for AC, it may not break short circuit current. Moreover, since tripping device specifications for some circuit breakers are different, it may not operate against overcurrent.
Product Name
Molded Case Circuit Breakers
Series
WS-V

May I have your opinion?

Inquiries