FAQ


FAQAbout Products

- FAQ > Low-voltage Power Distribution Products > Low-voltage Circuit Breakers > Accessories and Related Components > F-type and V-type operating handle
FAQ
F-type and V-type operating handle
What is the difference between F-type and V-type operating handle?
Answer
Both of F-type and V-type can remotely operate a circuit breaker in the panel board and the design of 800A fame or less are unified. Features are as follows.
*F-type control handle: It is installed on a circuit breaker itself
*V-type control handle: The handle part is installed on the door side of the panel board and mechanism part is installed on circuit beaker itself. (It is suitable for cases where the depth from the panel door to the mounting surface of a circuit breaker is deep)
*F-type control handle: It is installed on a circuit breaker itself
*V-type control handle: The handle part is installed on the door side of the panel board and mechanism part is installed on circuit beaker itself. (It is suitable for cases where the depth from the panel door to the mounting surface of a circuit breaker is deep)
- Product Name
- External Accessories
- Series
- WS-V