Start main contents

Factory Automation

Questions

  • No : 22402
  • Release Date : 2018/08/31 14:33
  • Print

ACB How to use MCR

What does MCR(Making Current release) mean?
Category : 

Answer

It is special relay characteristic for selective co-ordination. When closing ACB (changing from OFF to ON), the instantaneous tripping characteristic is effective, but after ACB closed, the instantaneous tripping characteristic becomes ineffective. Therefore, this instantaneous tripping characteristic control is useful for short-circuit fault protection when closing and to expand the selective coordination area with downstream circuit breaker. MCR function is provided in WS relay as option and in WB relay as standard. And instantaneous tripping or MCR is changeable by select switch.
Product Name
Low Voltage Air Circuit Breakers
Series
AE-SW
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?