Start main contents

Factory Automation

Questions

  • No : 22415
  • Release Date : 2018/08/31 14:33
  • Print

Where UVT power supplied from?

Is it possible to take power supply of UVT from the secondary side of a circuit breaker?
Category : 

Answer

Do not take the control power supply of UVT ("Resettable type" and "Reset prevention type") from the secondary side of the breakers. If taking the control power supply from secondary side of a circuit breaker, some problems may occurs (ex. resetting or making of a circuit breaker cannot be operated since the control voltage is not supplied to UVT when the circuit breaker is turned "OFF" or trips.
Product Name
Internal Accessories
Series
WS-V
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?