FAQ
FAQAbout Products
- FAQ > Low-voltage Power Distribution Products > Low-voltage Circuit Breakers > Accessories and Related Components > Fixed-type and Adjustable-type of V-type Operating handle
FAQ
Fixed-type and Adjustable-type of V-type Operating handle
What is the difference between Fixed-type and Adjustable-type of V-type Operating handle?
Answer
For Fixed type, the depth from the circuit breaker mounting surface to the panel board front is fixed. Adjustable-type is used when the depth from the circuit breaker mounting surface to the panel board front is deeper than Fixed type. It can be adjusted by cutting the shaft.(Max 300mm)
- Product Name
- External Accessories
- Series
- WS-V